Other Parts Discussed in Thread: SYSCONFIG
Hi. We have a problem on booting.
We make a custom board using am3352. we tested booting test at high temperature. The board was left in the chamber for one hour at 75°C and supply power.
At that time, some boards did not booting. we didn't receive any message from console. The boards operated normally at 25°C.
we use sysboot config '01011b' (usb0-> nand-> spi0-> mmc0). there was no device on the usb0. The booting data is in nand. usb0 is only used for testing and debugging.
I wonder why the board did not booting at high temperature.
Best Regards.