Other Parts Discussed in Thread: OMAP-L137, TMS320C6747, PCM1864
The documentation for this starter kit is very difficult to follow. I simply want help to get up and running with the OMAP-L137/TMS320C6747 Floating Point Starter Kit (SK) and the PCM1864 CMB as is demonstrated in the video demo .
I have installed CCS 8.1.0 but need help getting the correct Target Configuration as well as getting the demo projects loaded.
Here is the console message I get when trying to "connect to target.
"C674X_0: Error connecting to the target: Error 0x80000240/-1180 Fatal Error during: Initialization, OCS, The target is being held in reset. The applied reset must be released before progressing."