This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS: TDA2xx IPU M4 cache maintenance

Tool/software: TI-RTOS

Hello,

According to the TRM, there two sets of cache maintenance for the IPU M4:

one is under :

7.4.2.1 IPUx_UNICACHE_CFG Register Summary -

CACHE_MAINT                0x55080010     0x58880010
CACHE_MTSTART          0x55080014     0x58880014
CACHE_MTEND              0x55080018     0x58880018

and the second under:

Table 7-48. IPU1_UNICACHE_MMU (AMMU) Registers Mapping Summary - 

CACHE_MMU_MAINT            0x55080CA8         0x58880CA8
CACHE_MMU_MTSTART      0x55080CAC         0x58880CAC
CACHE_MMU_MTEND          0x55080CB0         0x58880CB0
CACHE_MMU_MAINTST       0x55080CB4          0x58880CB4

1. Can you please explain what is the difference between these two sets - what is the effect of each of them and when should each be used?

2. From looking at the PDK, it seems the unicache functions act on the first register set only - why?

3. What addresses the MSTART,MEND registers (for each of these sets)  should be written to -- physical addresses or virtual addresses (or it does not matter)?

4. For the first set there is no status register and looking at the PDK code it seems that, for example, the invalidate bit is expected to get cleared when invalidation is completed but I could not see the description/explanation on the TRM - can you please describe the full operation of this (and it this also true for the second set or for the second set only the status register should be examined)?

Thanks

Guy

  • Hi Guy,

    Cache maintenance registers are given in IPUx_UNICACHE_CFG space and are used for doing cache operations like preload, clean, etc.
    Hence PDK uses only first register set.
    You can write both physical and virtual addresses depending on AMMU configuration.
    For cache maintenance operations the expected behavior is as per PDK code. I will file a bug on TRM to update the description.
    I need to check with IP experts on CACHE_MMU maintenance registers.

    Regards,
    Rishabh
  • Hi,
    Thanks a lot for the info.
    Please update when you'll have more info regarding the CACHE_MMU

    Thanks
    Guy
  • Hi Guy,

    I checked with IP experts for these registers.
    CACHE_MMU maintenance registers are not relevant in the context of TDA SoCs.
    I will take an action to get them removed from the TRM.

    Regards,
    Rishabh