Part Number: AM3352
Tool/software: Linux
when I try to dump GPMC registers, u-boot is crashing.
In my code GPMC clock is already is active.
please help me....
Thanks
NU.
md 50000000
50000000: 00000060 00000000 00000000 00000000 `...............
50000010: 00000000 00000001 00000000 00000000 ................
50000020: 00000000 00000000 00000000 00000000 ................
50000030: 00000000 00000000 00000000 00000000 ................
50000040: 00001ff0 00000000 00000000 00000000 ................
50000050: 00000a00 00000001 00000000 00000000 ................
50000060: 28001000 00101001 22060514 10057016 ...(.......".p..
50000070: 010f1111 8f070000 00000f4a 00000000 ........J.......
50000080: 00000000 00000000 00000000 00000000 ................
50000090: 00001000 00101001 22060514 10057016 ...........".p..
500000a0: 010f1111 8f070000 00000f00data abort
pc : [<8ff9a568>] lr : [<8ff9a575>]
reloc pc : [<8082d568>] lr : [<8082d575>]
sp : 8df4cce0 ip : 00000000 fp : 500000a0
r10: 00000004 r9 : 8df4ced8 r8 : 500000ac
r7 : 00000003 r6 : 00000004 r5 : 00000004 r4 : 00000018
r3 : 8df4ccf4 r2 : 00000030 r1 : 00000000 r0 : 00000009
Flags: nZCv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
resetting ...
U-Boot SPL 2017.01-svn224 (Jul 15 2018 - 23:56:06)
Trying to boot from SPI
UID = 20BB1810_00002363_33761900_35002221_1016D7FE
U-Boot 2017.01-svn224 (Jul 15 2018 - 23:56:06 -0700)
CPU : AM335X-GP rev 2.1
I2C: ready
DRAM: 256 MiB
Reset PHY2...
Done