Hello Texas,
I'm doing a revision of a customized board with AM3352 + DDR3L, looking on the VREF your documentation recommends two resistors to provide a Vddq/2 on this pin. When checking the recommended values in the Schematic Checklist is considering 10k 1% values for these resistors, but when looking on datasheet of AM335x (Page 174 - Rev J) is recommended 1k 1% values.
Looking on BeagleboneBlack schematic (rev C) I've checked that is using the 10k 1% values (R98 and R100).
Considering another non-Ti documents, e.g: Micron reccommends 1k 1% value, guide (TN-46-14) page 5.
My question is, I believe both values will work, but what are the official recommendation from Texas. Is there any point of view for each weakness of these both options? Or is this just a mistake that has passed?