Dear Sir,
I can run my project well with emulator.
But when I boot my project from SPI flash, the UART interface would fail.
UART interface can work when I do : SPI boot --> Connect from emulator --> Load symbol --> Restart --> Run
I guess there is something set in the .gel file but I didn't set it in my project. I can not locate the missing setting.
Do you have any suggestion for this bug? Really appreciate your help!
Best Regards,
Eric Fang