Part Number: AM5728
Tool/software: Linux
Hi,
Attempting to compile & install modules using Processor SDK Linux 4.3 - install doesn't appear to work
I'm trying to rebuild the kernel, modules and device tree binaries by following these steps:
- make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- distclean
- make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- tisdk_am57xx-evm_defconfig
- make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- zImage
- make ARCH=arm CROSS_COMPILE=../../linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- am57xx-beagle-x15-revb1.dtb
- make ARCH=arm CROSS_COMPILE=../../linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- modules
This appears to complete with no issues. However, when I go to install the modules:
- export CROSS_COMPILE=arm-linux-gnueabihf-
- sudo make ARCH=arm INSTALL_MOD_PATH=/home/dmurphy/my_build modules_install
Unfortunately, the "sudo make ARCH=arm INSTALL_MOD_PATH=/media/rootfs modules_install" command from the link below doesn't actually install the modules in the INSTALL_MOD_PATH.
In fact, to run the command with sudo, I have to change the command to avoid gcc being picked up instead of the arm cross compiler:
sudo bash -c ' export CROSS_COMPILE=../../linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- ; make ARCH=arm INSTALL_MOD_PATH=/home/dmurphy/my_build/modules/ modules_install'
Regardless of whether I use sudo or not to make modules_install, nothing ends up in the INSTALL_MOD_PATH directory. After some time, the Make just ends abruptly with the following output:
...
CC sound/soc/generic/snd-soc-simple-card-utils.mod.o
LD [M] sound/soc/generic/snd-soc-simple-card-utils.ko
CC sound/soc/generic/snd-soc-simple-card.mod.o
LD [M] sound/soc/generic/snd-soc-simple-card.ko
CC sound/soc/omap/snd-soc-omap-hdmi-audio.mod.o
LD [M] sound/soc/omap/snd-soc-omap-hdmi-audio.ko
CC sound/usb/snd-usb-audio.mod.o
LD [M] sound/usb/snd-usb-audio.ko
CC sound/usb/snd-usbmidi-lib.mod.o
LD [M] sound/usb/snd-usbmidi-lib.ko
dmurphy@tibuilder:~/ti-processor-sdk-linux-am57xx-evm-04.03.00.05/board-support/linux-4.9.69+gitAUTOINC+9ce43c71ae-g9ce43c71ae$
Any assistance would be greatly appreciated.
Thanks,
Dermot