Part Number: AMIC110
Hello everyone,
we are going to develop an industrial ethernet solution.
We want to make an allready existing device able to be used as a EtherCAT-Slave / Profinet Device, this device only has an SPI-Interface with a fix protocol awaylable.
Is it possible to use the AMIC110 without an additional Host-Processor to convert the Industrial Etherent into the fix SPI-protocoll or is an external Host-Processor nedded.
(Write own firmware running on the AMIC110 which does exactly this)
If it's not possible with the AMIC110, which TI device is capable of doing this task?
Regards,
Marcel Kummer.