This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4377: Debug UART issue

Part Number: AM4377
Other Parts Discussed in Thread: AM4379, TXS0102

Hi Team,

We are using AM4377 processor and FT232RQ USB-UART converter in one of our projects. We are facing some issue with this device and issue description is as below:
We are finding 0.6V to 0.9V on board's 3.3V power rail without powering on the board when we connect it to PC/Laptop. We have seen this in few boards (AM4377, AM4379 etc). So, some interfaces are getting affected by this as power ramp is not from 0 to 3.3V but from 0.9V to 3.3V. This is because there is 1V-3V on UART0 TX & RX lines (different in different boards). How voltage on UART0 TX RX is affecting 3.3V power rail? Is it connected through some channels internally ?

Best Regards,
Madhusoodana Bairy