Hello,
I am writing program in kernel C. I need to division operation.
As there is no division operation available , tring to use right shift ( >>) for same.
But getting below error,
76. diffOut = vin1 >> 2; // line in code
Error :-
"../practice1.k", line 76: error #26001-D: syntax error near 'vin1'
"../practice1.k", line 76: error #26001-D: syntax error near 'vin1'
"../practice1.k", line 76: error #26001-D: syntax error near ';'
So want to know that,
1. Is right shift support available ?
2. Is compiler doesn't support division operation because of result maybe in floating point ? (if so , right shift should work!!)
Any suggestion to do division operation!!