This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6446EVM example source code for the "video_loopback"

Hi all,

How can i get the source code for the video_loopback which is included in DM6446EVM board support package fiie "SetupDavinciEVM-Release321.exe".

It has only executable binary file, not source code. On the other hand , in DavinciHD-EVM , it has full source code for examples.

best regards,

G.S.Lee

  • Unfortunately the source code for the SD board support package for DM6446 is not available, though it is for other platforms as you have noted.

    Typically I would suggest using the Linux drivers that are included with the DVSDK, however if you need a low level test like this than you may want to look at the board support source code for the DM355 which has a similar VPSS.