Can the C674x DSP be booted while keeping the ARM inert (in reset)?. To put it another way, can you use this chip, pretending that it just has the DSP in it and no ARM?.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the C674x DSP be booted while keeping the ARM inert (in reset)?. To put it another way, can you use this chip, pretending that it just has the DSP in it and no ARM?.
So you cannot run a simple "Hello World" app from CCS via the JTAG on the c6a816x evm? Instead, you have to use Syslink's ProcMgr to attach to the DSP, load a code image, and then start it up:
ProcMgr_open
ProcMgr_attach
ProcMgr_load
ProcMgr_start
When in this sequence may the JTAG be brought in to see what the DSP is doing?
Lee Holeva
Lee,
ProcMgr_start releases the DSP from reset. So you can connect to the DSP after ProcMgr_start has completed successfully.
Regards,
Mugdha