Part Number: AM5728
Tool/software: Linux
Hi TI Experts,
I have below questions about AM5728
Q1. Can MPU and DSP run at the same time and independently?
Ex : Run Linux in MPU, Run RTOS in DSP at the same time?
Q2.Can I use DSP of AM5728 as CPU function?
Q3.There are three kind of OS provided in TI.com (below list), is there any rule to use these OS in MPU & DSP of AM5728 ?
(1) Linux Processor SDK for AM57x
(2) Linux-RT Processor SDK for AM57x
(3) RTOS Processor SDK for AM57x
For exampie : Linux only can used in MPU, or RTOS only used in DSP ?
If yes, could you please provide the limitation rule to me?
Q4. For above three OS, do these OS support all the TI processor (A9, A15, A53...) ?
Q5. If we want to study TI RTOS and use a simple EVM to implement.
Could you suggest simplest/cheapest EVM to me?
Thanks a lot.
Derek