Other Parts Discussed in Thread: TMS320C6424, TMS320DM647
hello all,
i am looking for board DM648, initially i was working on TMS320C6424. i was given the task to complete the full duplex communication. i was receiving LAN data from E MAC of evm6424 and transmitting it on LAN back through a daughter card. i have two RJ45 for full duplex communication, one on evm6424 and other on the daughter card.
the problem was that data transfer between evm6424 and daughter card was through SPI. SPI has a max data transfer rate of 15 Mbps, which is insufficient for 100 Mbps LAN transfer.
now i as looking at DM648, which has two ports. i have some queries before i purchase new board...
does its both ports or say G Macs work simultaneously?
had anyone did the job as i want to do?
does this board solves my problem of real time traffic, picking all packets from one port and transmitting to other port and vice versa without delay?
regards
adnan khurshid