Hello all,
I have problem to connect DM6446EVM and CCS3.3
on running CCS3.3 , it warns to "Error initializing emulator".
Next is my configurations. Is there my mistake?
1. CCS 3.3 and 6446EVM-revD (dark green solder mask PCB)
2. CCS service pack 12. fn:SR12_CCS_v3.3_SR_3.3.82.10.1.exe
3. XDS560R driver. fn : setupXDS560RCCSPlatinum_v30329A.exe
4. board support. fn : SetupDavinciEVM-Release321.exe
5. S3:
/----------\
| # OFF ON |
-| 1 X |- Boot mode
-| 2 X |- "
-| 3 X |- 8/16 bit bus
-| 4 X |- DSP boot
-| 5 X |- EMIF ADDR lines
-| 6 X |- "
-| 7 X |- "
-| 8 X |- "
-| 9 X |- "
-| 10 X |- User SW
\----------/
this is S3 dip switch configuration from \boards\davincievm\ReadMe.html
6. the EMU1 and the TRSTn dip switchs are set to the left side.
7. CCSetup.
best regards,
G.S.Lee