Hello TI Experts,
I am creating a library to DSP, I used C6Run v0.94.03.03 and everything ok, but if I use C6Run v0.94.04.05, the script c6runlib-cc generates the next error:
Can't call method "root" on an undefined value at /home/mleiva/C6Run_0_94_04_05/bin/../bin/perl/c6runlib-rpcgen.pl line 1223.
/home/mleiva/C6Run_0_94_04_05/bin/c6runlib-cc: line 447: /opt/arm-linux-gnueabi: is a directory
/home/mleiva/C6Run_0_94_04_05/bin/c6runlib-cc: line 455: /opt/TI/TI_CGT_C6000_6.1.9: is a directory
/home/mleiva/C6Run_0_94_04_05/bin/c6runlib-cc: line 469: /opt/TI/TI_CGT_C6000_6.1.9: is a directory
mv: cannot stat `pcuDsp.o': No such file or directory
mv: cannot stat `pcuDsp.gpp_stub.o': No such file or directory
mv: cannot stat `pcuDsp.dsp_stub.o': No such file or directory
c6runlib-ar: dspobj/pcuDsp.o: No such file or directory
What's wrong?
Thanks.