Part Number: AMIC110
Other Parts Discussed in Thread: AM3357, AM3359
Hi All,
We want to use AMIC110 for our application using SPI interface.
Below are the clarifications,
#In AMIC110, for Stack code compilation, Do we need to use Beckhoff Ethercat SSC Tool?
# For AMIC 110, which option needs to be selected for custom Slave code generation option? Currently, there is no dedicated option available for AMIC110. TI AM335x Sample option only available.
A full featured EtherCAT Industrial example uses Patches for the Beckhoff Slave Stack Code(SSC 5.11) that enable the SDK to build a full featured EtherCAT application which can be customized as described in the processors.wiki.ti.com
I got the above statement from wiki.ti.com.
Can you please brief on this? When do we need to go? Is there additional charges needs to be paid for ETG?
Regards,
S.Saravanakumar