Other Parts Discussed in Thread: TLV320AIC3204, TPS62260
I'm seeing random "drop outs" of the 1.8 volt supply every 100 to 300 ms that last for a duration of roughly 20 to 30 ms where the voltage drops to less than .1 volts. This is on one of TI's TMS320C5535 eZDSP cards. The 3.3 volt supply works fine which is derived from the same 5 volt supply from the USB connector. Also, the software running on the DSP works fine on other eZDSP cards. And, on this card, the DSP is able to boot up from the micro SD card, re-encrypt the "requesting to be bound" code on the microSD card, and write it back to the card, all before these 1.8 volt "pulses" start to occur. Once that is done, all four LEDs in the middle of the board stay on and the green LED on the XF pin "flickers".
This same software worked fine on this board for at least for a couple weeks of operation, and also works fine on other 5535 eZDSP boards. The 1.8 volt supply on the eZDSP card connects to the LDOI pins ( B14, C14, and B10 ) of the DSP and also the DVDD and AVDD pins on the TLV320AIC3204 codec so it potentially could be either part that "went bad".
Any information or help in debugging would greatly be appreciated!
Tom