Other Parts Discussed in Thread: OMAP3503, OMAP3530
Hello Champs,
Does OMAP3503 support SD card detection using a DAT3 pin?
Best regards,
Nori Shinozaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can someone check on this?
I heard DaVinci Processors can use the DAT3 pin for a card insertion and ejection.
Regards,
Nori Shinozaki
Nori Shinozaki said:Hello Champs,
Does OMAP3530 support SD card detection using a DAT3 pin?
Best regards,
Nori Shinozaki
This should be possible on OMAP3. However, I think it requires some controllable external hardware to do the detection, or at least be able to enable/disable pull up/down resistors on that pin, which is possible on OMAP3.
Regards,
James