This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5726: Secure boot

Part Number: AM5726


Tool/software: Linux

Hello,

I am using am5726. Kernel ver is 4.4.32.

I want to encrypt one partition of the filesystem. 

What is the procedure for that?

Regards,

Prerak

  • Prerak,

    You can use dm-crypt.

    In userspace you will need package  lvm2 and cryptsetup, but I don't think they are provided in the Processor SDK filesystem. So you will have to compile them from source code or yacto.

    In kernel please enable Device Mapper is enabled in kernel config.

        Device Drivers  --->                                                           
            [*] Multiple devices driver support (RAID and LVM)  --->                   
                <*>   Device mapper support                                            
                [*]     Device mapper debugging support                                
                <*>     Crypt target support