This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3G support in DaVinci



We are developing a SDI Board with TMS320DM6467CZUT7 and GS2972 (SDI Transmitter, Mnfr: Gennum Corp). TMS320DM6467CZUT7 will be used as Video Pattern generator and GS2972 serializes the digital bit patterns. The VPIF bus is interfaced between both. I am expecting to generate 3G stream out with the help of TMS320DM6467CZUT7. When checking GS2972 the device has the capability to support 2.97Gbps data in SMPTE 424.

By verifying the VPIF guide of TMS320DM6467CZUT7, I can find that BT.1120, BT656 and SMPTE 296M modes only getting supported.

  1. Is the TMS320DM6467CZUT7 Pxr VPIF supports for 3G (SMPTE 424).
  2. How the VPIF Clock can be increased to 150MHz. 

If the PXR TMS320DM6467CZUT7 is not supporting for SMPTE 424 , Pls let me know the alternative