Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3352, AM3359,
Tool/software: Linux
Hi,
We currently have application running on the AM3352 Sitara series running a Linux Host and need to add the PRP functionality and looking at various options to implement the same. This is for substation automation industry.
I went through the training videos on : HSR and PRP Redundancy on RT Linux . There was a mention in Redundancy and Linux section in that the TI designs on PRP and HSR are currently working on TI-RTOS and TI will be working on updating those to Linux in the near future. Do you have a timeline for when this will be available , and also if this support will be available for AM3359 ?
I also did go through the training videos for PRP TI Design using PRU-ICSS. I wanted to know if TI has done any evaluation/comparison of PRP's LRE being implemented in PRU-ICSS as compared to LRE as part of the network stack in Linux. Any recommendation on which one is better wrt latency in processing of packets?
I am trying to make a decision on whether to update the processor to AM3359 so we have the option to implement the TI PRP in the PRU-ICSS or to go ahead and add the LRE network stack in the Linux kernel to our existing design. We currently use mainline Linux and will have to update it to RT-Linux for better deterministic latency.
Thanks,
Prema