Tool/software: Linux
I am trying to configure a USB serial console by the following defines.
#define CONFIG_MUSB_UDC
#define CONFIG_USBD_HS
#define CONFIG_USB_TTY
#define CONFIG_SYS_CONSOLE_IS_IN_ENV
I get the following unresolved references in udc_init
musb/musb_udc.c:939: undefined reference to 'musb_platform_init'
musb/musb_udc.c:959: undefined reference to 'musb_cfg'
Looking at the musb_udc.c file where the udc_init function resides it has the following
#if defined(CONFIG_USB_OMAP3)
#include "omap3.h"
#elif defined(CONFIG_USB_AM35X)
#include "am35x.h"
#elif defined(CONFIG_USB_DAVINCI)
#include "davinci.h"
#endif
I don't believe any of these files are applicable to the am437x
Has anyone tried configuring a USB console on the AM437X platform