Hello.
I have encountered problem that HECC bit timing is extended at ERM=1.
I confirmed it on AM3517EVM which just connect #2pin and #3pin of J36 on the application board.
And I used AM35xx BSL and test program which can download in the Logic PD site.
- 1013707A_AM35xx_BSL.zip\bsl\lib\evmam35xx_bsl.lib
- 1013707A_AM35xx_BSL.zip\tests\evm\can
Because default bit rate is 0.8125MHz in test program, pulse width represents 1.23usec in ERM=0.
But, it changes into 1.38usec when I set ERM=1.
Because bit timing delay exceeds receiver acceptable timing by environment effects, I am really embarrassed.
Could you help me please?
1) Does the HECC adjust rising edge time of the transmit data at ERM=1?
2) Please teach me if there are something restriction about this.
3) Or, I would like to clarify this problem is never happen at ERM=0.
Best Regards,
BL.HSR-WZ