This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6747: How do I decide the proper value of McASP X/RCLKCHK Registers?

Part Number: TMS320C6747


Hi Sahin,

I'd like to ask you again.
I think that I understand what you said. But I need a example in detail. Could you please show me it?

Regards,
j-breeze

  • Hi,

    The sw team is notified.

    Best Regards,
    Yordan
  • Hi Yordan,

    I do not think it relates to software. However, I am still expecting the response regarding this issue from the sw team.

    Regards,
    j-breeze

  • Hi,

    Could you please let me know the current status regarding this thread?

    Regards,
    j-breeze

  • The configuration of this register requires you to do some math to compute what is the eventual baud rate that is required for your application.

    You start with the sampling rate of your audio and then use the information regarding whether 32 bit data or 16 bit data is used and the slot size that you use with the peripheral.

    BIt rate = sampling rate * number of slots * size of each slot

    Check out the discussion here:
    e2e.ti.com/.../562633

    In order to simulate module clocks, we provide a clocking spreadsheet where, if you setup the PLLs, you can try to setup the MCASP internal dividers to obtain the eventual transmit or receive bit clock that you want to use as per your usecase.
    processors.wiki.ti.com/.../AM18xx

    I recommend that you check this tool out as it provides good visualization of how the MCASP and devices clocking works.

    Regards,
    Rahul
  • Hi Rahul,

    Thank you for your reply, but I think it seems that you are misunderstanding.
    I'm asking about McASP X/RCLKCHK Registers.

    I'm not sure that how I decide the poper XMAX/XMIN field values.
    Could you please let me know the formula to calculate the values?

    Regards,
    j-breeze

  • J-Breeze,

    I am sorry, I misinterpreted the question. The Transmit Clock Failure Check and Recovery is usually used to detect a clock stop condition or when an external high clock is provided in the system and you want to ensure that there is no large variation in the in clock. 

    the setting for XMIN and XMAX is totally dependent on the condition that you are trying to catch. For example, you need to first find out what the MCASP module clock value(using internal clock or AUXCLK) is as this is the system clock tick that is used to calculate XCNT.  this clock counts 32 high rate AHCLKX clocks. 

    for setting this to catch any errors, I would recommend that in your setup when the clock is running normally, read the value of XCNT and based on that value you need to calculate the maximum tolerable deviation to setup XMIN and XMAX. This mechanism is described in fair amount of detail in the Clock Failure Detection of the MCASP chapter in the TRM.

    for detecting clock stop condition, you can set the XMIN to 1 as when the AHCLKX clock stops, the count detect will be zero and will be less than 1 setup so will be enough to catch the clock failure condition. In order to catch incoming clock frequency variations, you may need some trial and error to set the correct XMIN and XMAX values based on XCNT value detected during normal condition.

    Regards,

    Rahul

  • Hi Raful,

    I checked an old example called QuickStartOMAPL1x rCSL and found a code for the clock failure check below in it.
    Can I refer to it?

      o quickStartOMAPL1x_rCSL_2.0
        (software-dl.ti.com/.../quickStartOMAPL1x_rCSL-2.0-Setup.zip)

      o mcasp.c
        (C:\ti\quickStartOMAPL1x_rCSL\OMAPL1x\rCSL_examples\evmOMAPL138\DSP_examples\mcasp)

        - Line 446~477

          //Transmit Clock Check Control Register

          //Set McASP Clock Zone Post Scaler

          //Note McASP is driven by SYSCLK2 which is SYSCLK/ which is a divide
          // by two of the main system clock 300/2 = (150MHz)
          CSL_FINST(mcaspRegs->XCLKCHK, MCASP_XCLKCHK_XPS, DIVBY4);

          //Set XMAX Value
              //Notes: Prescale by 4
              //150/4 = 37.5 MHz

              //37.5MHz /24.576MHz (AUXCLK)  = 1.52587890625
              //32 Clock Counts * 1.52587890625 = 48.8 McASP System Clock Counts per every 32 AHCLKX
              //Counts

              //___________________________________________
              //32 ACLKs / 24.576MHz = 1.302uSec
            
              //48 Clocks / 37.5 MHz = 1.28 uSec
              //49 Clocks / 37.5 MHz = 1.306uSec
        
              //___________________________________________
              //Check
              //1.28 uSec < 1.302uSec < 1.306uSec
        
              //Include clock count buffer of 1 CLOCK
              //So Configure XMIN to be Uint8 47 (0x2F)
              //   Configure XMAX to be Uint8 50 (0x32)
     
          CSL_FINS(mcaspRegs->XCLKCHK, MCASP_XCLKCHK_XMIN, 0x2F);    
          CSL_FINS(mcaspRegs->XCLKCHK, MCASP_XCLKCHK_XMAX, 0x32);
     
    Regards,
    j-breeze




  • J-Breeze,

    The code provided in Quick Start guide is legacy code that we are no longer maintaining. The code was created in 2010 time frame and tested on the EVM so it can be used as reference but we are not in a position to support questions based on that code. It does seem to have the relevant code setup that you were looking for but every audio system/clock setup is different to and may have have different sensitivity to clock variation than what is described in that example so while you can use the code, the values of XMIN, XMAX may need to change based on your design.

    Regards,
    Rahul
  • Hi Rahul,

    Thank you for your advice. I have one more question.
    Could you please let me know what the clock count buffer is? Do I have to include it to calculate the XMAX/XMIN field values?

    Sorry to bother you, but I'd like to ask you about it because it's a McASP Hardware spec,  not related to the code.

    Regards,
    j-breeze

  • I have contacted the hardware team since this is an internal design question. I have not heard back and they will reply to the post directly.

    Regards,
    Rahul
  • Hi j-breeze,

    I think the term "clock count buffer" is a little confusing, because people usually mean "memory space" or something similar when they use the term "buffer."  In this case, I think the coder just meant "margin."

    The calculations in this example tell you that you want 48.8 system clock counts per 32 AHCLKX counts - that's your ideal, correct count.  You could check that your clock count measurement (XCNT) is between 48 and 49, but that means that your ideal count (48.8) is within only 0.8 counts of the min (48), and only 0.2 counts of the max (49); when you're working with integers, there's nothing between 48 and 49.

    You should allow for a margin of at least one clock in each direction.  You do that by adding one clock count to the max boundary and subtracting one clock count from the min.  Therefore instead of:

    48 < 48.8 < 49

    you'd add that one clock count "buffer" in each direction and get:

    47 < 48.8 < 50

    Basically as long as your count is 48 or 49 clocks, you'll be OK.

    Hope this helps.