Part Number: AM3358
Tool/software: Linux
Hi ,
I am trying to boot my customized board through sdcard(mmc0), in u-boot i am trying to check the information of mmc0 by using below command, but it is giving below error, could you please help me on this
U-Boot SPL 2018.01-dirty (Jul 30 2018 - 15:56:53)
Trying to boot from UART
CxyzModem - CRC mode, 3305(SOH)/0(STX)/0(CAN) packets, 4 retries
Loaded 422888 bytes
U-Boot 2018.01-dirty (Jul 30 2018 - 15:56:53 +0530)
CPU : AM335X-GP rev 2.1
I2C: ready
DRAM: 512 MiB
No match for driver 'omap_hsmmc'
No match for driver 'omap_hsmmc'
Some drivers were not found
Reset Source: Global external warm reset has occurred.
Reset Source: watchdog reset has occurred.
Reset Source: Power-on reset has occurred.
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
BeagleBone: cape eeprom: i2c_probe: 0x54:
BeagleBone: cape eeprom: i2c_probe: 0x55:
BeagleBone: cape eeprom: i2c_probe: 0x56:
BeagleBone: cape eeprom: i2c_probe: 0x57:
Net: usb_ether
Press SPACE to abort autoboot in 2 seconds
=> mm
mm mmc mmcinfo
=> mmc
mmc mmcinfo
=> mmc info
mmc_read_data: timedout waiting for status!
omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear
omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear
omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear
Device: OMAP SD/MMC
Manufacturer ID: 0
OEM: 0
Name: Tran Speed: 25000000
Rd Block Len: 512
SD version 1.0
High Capacity: No
Capacity: 121.3 MiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
=>
Regards,
Anantha