Hi, I have been using a C6713 DSK for about two years now and have found all these resources excellent. Thank you so much for giving your time to help out us all. However, I have not been able to find an answer to this issue. Another forum (DSP Related) recommended posting here.
I wish to send data from the PC to the transmitter DSK (no 1) and then retrieve data from the receiver dsk (no 2) to the PC. Can I use the RTDX usb interface to do this?
I mention RTDX because the API appears to have a board name property. However the manual for RTDX does not expand on this.
Another approach I have used is the CCS Version (2.21) Configuration Tool and placed two configurations of the same DSK (Just the names are different. Upon starting I get the CCS: Parallel Debug Manager. My understanding is this allows me open an instance of CCS for each DSK. When I go to Group>>edit it only shows First Board and I can change which DSK configuration it should use. How do I get the second DSK to appear in this list?
Lastly, are there other methods to allow this type of interfacing between one PC and two DSKs? I have considered serial but I do not currently have the funds for serial daughter boards.
Thanks,
James
###Update##'
I have used a different PC today which had Code Composer 3.2V installed. The Parallel Debug Manager is a bit more functional. Basically, it allowed me to connect to DSKs real targets. However, when I did a quick test (gel menu) in each code composer instance it was communicating with the same board (only one board). Confirming in windows device manager that both had found the driver successfully - which they had I can only assume the Spectrum Digital DSK driver (or was it made by TI?) is not designed to work with multiple DSKs. I noticed in the PDM that I could change the port number - which is currently identical (unsurprisingly). But what would I change the second DSK port number too?
Lastly, someone on DSP related said they believe there might have been a 'hack' to get code composer to work with multiple DSKs. I have since found similar questions from the past on various forums - all went unanswered. please help.
How can I use only one PC to communicate with two DSK boards? any solutions?
thankyou so much
james