Part Number: DRA72
Other Parts Discussed in Thread: TPS61196
Tool/software: Linux
Our DRA726 boards use either a 12 inch or 7 inch display from US Micro. I control the backlight with ehrpwm0
In my device trees I have this for the backlight
lcd_bl: backlight {
compatible = "pwm-backlight";
pinctrl-names = "default";
pinctrl-0 = <&bl_pwm_pins>;
pwms = <&ehrpwm0 0 50000 0>;
enable-gpios = <&gpio6 6 GPIO_ACTIVE_HIGH>;
/* 0 to 255 */
brightness-levels =
<0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19
20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39
40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59
60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79
80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99
100 101 102 103 104 105 106 107 108 109 110 111 112 113 114 115 116 117 118
120 121 122 123 124 125 126 127 128 129 130 131 132 133 134 135 136 137 138
140 141 142 143 144 145 146 147 148 149 150 151 152 153 154 155 156 157 158
160 161 162 163 164 165 166 167 168 169 170 171 172 173 174 175 176 177 178
180 181 182 183 184 185 186 187 188 189 190 191 192 193 194 195 196 197 198
200 201 202 203 204 205 206 207 208 209 210 211 212 213 214 215 216 217 218
220 221 222 223 224 225 226 227 228 229 230 231 233 232 234 234 236 237 238
240 241 242 243 244 245 246 247 248 249 250 251 252 253 254 255>;
default-brightness-level = <127>;
};
The problem I have is the same for both, for a brightness from 1 to 6 I get 100% brightness.
I was suspecting a bug in the application so I check on the command line and I get the same results.
root@actia-dra726-12inch:/sys/class/backlight/backlight# echo 6 >brightness
root@actia-dra726-12inch:/sys/class/backlight/backlight# cat brightness
6
root@actia-dra726-12inch:/sys/class/backlight/backlight#
If I set to 0 the screen goes black which is what I expected.
If I set to 7 the screen has low brightness as expected
Michel Catudal
ACTIA Corp