Hi,
I have been trying to use AISgen and SPI Flash Writer to burn a program into flash memory on a C6748 but have encountered difficulties.
Using logic EVM with C6748 SOM.
Have a working .out file (that I can load and run from CCS) and this includes calls to functions EVMOMAPL138_init() and EVMOMAPL138_initRAM().
Have used AISgen for D800K006 to create .bin file. Device Type (according to memory location 0x11700000) is d800k004. In AISgen application I entered this information along with DSP, Boot Mode: SPI1 Flash, Clock Source: Crystal 24MHz, but didn't check any of the Configure PLL0, etc. boxes.
approx 40kB .bin file produced.
Loaded and ran SPIWriter_OMAP-L138.out (from OMAP-L138_FlashAndBootUtils version 2.29).
Answered 'n' to first question.
Four minutes later, message 'INFO: File read complete' appeared.
SPIWriter program continued running but after half an hour and no further messages I halted it.
Any help appreciated. Is this anything to do with the XDS100v1 JTAG interface?
Donald