This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Are there any details in loading code to DM365 IRAM with slh_36x?



I have a problem with loading pretty simple program (toggling GIO) to IRAM (DM365 on EVM) with slh_DM36x utility. Same piece of code (a dozen of instructions) works when loaded using slh_36x -load2DDR or uboot. Are there evident details I'm missing?

PS. I mean I have problem with running the code - load process looks fine.

    /* Toggling GIO 26 */
_start:
    MOV        R1, #0x01C40000            /* Load base address of system module */
    ADD        R1, R1, #0x0C                   /* Add offset for PINMUX3 register */
    LDR        R2, [R1]                               /* Reading PINMUX3 */
    AND        R2, R2, #0x7FFFFFFF     /* Clear bit 31 of PINMUX3 */
    STR        R2, [R1]                               /* Write back PINMUX3 - now pin U1 is GIO26 rather then SPI */
set_dir:                                                    /* Set pin as an output */
    ADD        R1, R1, #0x00027000     /* Shift pointer to GPIO registers */
    ADD        R1, R1, #0x00000004     /* To DIR01 */
    LDR        R2, [R1]                              /* Read DIR01 */
    AND        R2, R2, #0xFBFFFFFF    /* Clear bit 26 */
    STR        R2, [R1]                              /* Write DIR01 back - GIO26 is an output*/
    ADD        R1, R1, #0x00000008    /* Shift pointer to SET_DATA01 register */
set_bit:
    MOV        R2, #0x04000000
    STR        R2, [R1]
clr_bit:   
    ADD        R1, R1, #0x00000004
    STR        R2, [R1]
    SUB        R1, R1, #0x00000004
    B        set_bit