Hi,
My customer has bought a C6455 Evaluation Module along with XDS560 emulator. When he tried to launch & connect CCS, after installing all the provided software, it failed giving the following error:
1) 0x80002280/-1260- Fatal Error During Target Communication
2) 0x80000240/-1166- Invalid data scanned by the emulation controller
The same error keeps coming everytime. We tried communicating with the DSK through the embedded JTAG emulator as well as the external emulator but failed. I tried connecting the daughter card as well but that didn't make any difference. All the switch settings are the default ones.
A basic test utility also gets installed when CCS was installed. This could be used to test various peripherals like DDR etc. When this is tried, it failed in the very first step saying that USB connection is not proper and tests could not proceed further. All the software was re-installed as well but no luck.
I tried going through the documentation coming along with the kit but could not find much.
Has anyone faced this problem earlier? Are there any switch settings which are stopping CCS to communicate with the EVM? Please help as the customer is blocked and could not proceed further.