Other Parts Discussed in Thread: AM5718
Hello,
I have been trying to set up a boundary scan test on one of our new board configurations that is using the AM5716 processor. We are using this processor as a drop-in replacement for AM572x which we have been using in boundary scan mode with no major issues. However, when I tried to set up the test using the AM5716 I ran into several issues I was not able to resolve, related to the following pins:
ddr1_csn0(#AH23)
ddr1_wen(#AH21)
ddr1_dqs_ecc(#V27)
gpmc_a7(#P5)
gpmc_a13(#R3)
gpmc_a18(#R2)
gpmc_a23(#J7)
gpmc_wen(#M3)
mmc3_clk(#AD4)
uart1_ctsn(#E25)
These pins are able to read signal levels driven by our external test PLDs without issue, but the external PLDs continue to read low signal level when driving high from the AM5716. These pins are not called out anywhere in the AM572x/1x compatibility guide, and as far as I can tell there was no change in boundary scan or signal level for these pins that would explain the issues we are seeing. The behavior is consistent between several of our debug boards. As I mentioned above, we are testing these signals on AM572x without issue.
Let me know if you have any ideas why this might be happening, how to solve it, or if you need any more information.
Regards,
Joshua Nejedly