Hello:
I am getting the following linker error on a DM6437. CGTools 6.1.7. The code is using C++ and Templates, with Compiler "Memory model" = "Far Aggregate" or = "Far" (We didn't have this problem with v6.0.8).
That relocated address seems suspicious since it isn't 0x8xxxxxxx or is that an offset? It doesn't make sense as an offset either.
Thanks,
--B
"C:/Program Files/C6000Code Generation Tools 6.1.7/include/limits", line 316: warning: relocation from function "Engine::init" to symbol "_init__Q2_3The31Converter__tm__7_5TiC64FPCQ2_3The7XMLNode_v" overflowed; the 31-bit relocated address 0xdeffb0c0 is too large to encode in the 21-bit signed PC-Relative field (type = 'R_C60PCR21' (82), file = "D:\\testCCS\\bin\\lib\\c64\\Debug\\engine.lib<Engine.obj>",offset = 0x00011d0c, section = ".text")