I need to transfer about 200KByte from the local memory of the e5515ezdsp (stored in the internal SARAM) to a file on Windows
I am using "memory save" from the memory view defining start address and length
The transfer is executed but it takes several minutes which is not acceptable in my setup
Is there any faster way to transfer data from memory to host ?
This is not a communication bandwidth problem as USB2.0 should be able to transfer this amount of data in seconds
Thanks
Zeev