Part Number: AM3352
Hi Sir
we set E17 as GPIO to control TLP291 device.
below is the schematic
1. we measured the U910 pin 1 and the current is over 25mA.
2. we removed R915 and found the current of U910 pin 1 is 2.5mA.
3. we replace U910 device with a new one and the result is the same.
It means the max current of pin E17 of AM3352 is over the max. current 4mA.
Could you advise why E17 pin can offer the current over the spec?
BR
Yimin