Other Parts Discussed in Thread: TPD1E05U06
Is there any special reason why HDMI differential signal pairs CPU_HDMI_TX[0-2] and CPU_HDMI_TXC do not go through companion IC TPD12S016RKTR prior to external connector?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any special reason why HDMI differential signal pairs CPU_HDMI_TX[0-2] and CPU_HDMI_TXC do not go through companion IC TPD12S016RKTR prior to external connector?
The TPD12S016RKTR had too much capacitance for the TDA2 HDMI signals, and could not meet the HDMI electrical specifications. TPS12S016 data sheets states typical capacitance is 1.2pF. The ESD components used on the EVM (TPD1E05U06) has typical capacitance of 0.42pF. Additionally, the EVM implements voids in the ground plane beneath the ESD diodes to minimize the capacitance even more.
Thanks
Robert