This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP/BIOS, General PRD Interrupts Question. Missing PRD (DM6437)



I have a periodic timer that seems to be getting delayed or missed. 

bios.CLK.instance("PRD_clock").order = 1;
bios.PRD.create("PRD0");
bios.PRD.instance("PRD0").order = 1;
bios.PRD.instance("PRD0").mode = "continuous";
bios.PRD.instance("PRD0").period = 8;
bios.PRD.instance("PRD0").fxn = prog.extern("periodicTimeUpdate");

(Software pipelining (-mu) is off).

On the execution graph I see it run every 8 ms (as designed), except occassionally when I a big gap where it was obviously missed/delayed.  In the "gap" I see a lower priority task running.   One thing that strikes me as odd is that there are many many SEM_posts of an unknown handle shown on the graph at the time I would expect the periodic timer run. 

Can SEM_posts cause a periodic timer to be skipped or dropped?   WHat is this DSP/BIOS SEM_post?

Execution Graph Detail Says.
45346624 PRD: begin PRD0 (0x852214ac)
45346625 PRD: end

45346626 SWI: end PRD_swi (0x852213ec) state = done
45346627 SWI: begin KNL_swi (TSK scheduler) (0x852213c0)
45346628 SWI: end KNL_swi (TSK scheduler) (0x852213c0) state = done
45346629 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346630 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346631 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346632 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346633 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346634 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346635 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346636 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346637 SEM: post <unknown handle> (0x850e2aa0) count = 0
45346638 SEM: post <unknown handle> (0x850e2aa0) count = 0

Map file says...

                  850e2aa0    00000028     bios.a64P : tsk_stup.o64P (.far)