I am using DVSDK 3.10.00.12 on a DM365 EVM, and we are capturing video with the camera interface (connector J10) and displaying video using the composite output. We would like to switch to using the LCD output in YCC16 mode. However, I don't see an example of anything being used other than component or composite video output. How do you setup the display driver to output in YCC16 mode on the LCD output?
And when the LCD output is being used, how do you set the display frame rate? We're only capturing frames at 10 frames per second, so we'd like to slow down the video display to match.