Part Number: TDA2P-ACD
Other Parts Discussed in Thread: TDA2
Tool/software: Linux
Hello,
We have a custom board with TDA2P SoC and running Linux on A15.
There is NAND flash( MX30LF1G18A) connected to TDA and want to access it from U-boot.
We have configured the NAND driver in U-boot and also added the gpmc node to the dts file and enabled the pinmux config.
When we run the code we see U-Boot log and code hangs at NAND probing.
Here is the Uboot log :
U-Boot SPL 2016.05-00010-g9551b3d-dirty (Aug 06 2018 - 12:42:11)
DRA762-GP ES1.0
board_init
********spl_boot_device******no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
*** Warning - MMC init failed, using default environment
i2c_write: error waiting for data ACK (status=0x116)
i2c_write: error waiting for data ACK (status=0x116)
********spl_boot_device******Trying to boot from spl MMC1
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
spl: falcon_args_file not set in environment, falling back to default
reading single-stage-boot.dtb
spl_load_image_fat_os: error reading image single-stage-boot.dtb, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-00010-g9551b3d-dirty (Aug 06 2018 - 12:42:11 +0530)
CPU : DRA762-GP ES1.0
Model: TI DRA762 EVM
Board: DRA74x EVM REV
DRAM: 512 MiB
NAND:
DTS config for GPMC:
&gpmc {
/*
* For the existing IOdelay configuration via U-Boot we don't
* support NAND on dra72-evm. Keep it disabled. Enabling it
* requires a different configuration by U-Boot.
*/
status = "okay";
ranges = <0 0 0x08000000 0x01000000>; /* minimum GPMC partition = 16MB */
nand@0,0 {
/* To use NAND, DIP switch SW5 must be set like so:
* SW5.1 (NAND_SELn) = ON (LOW)
* SW5.9 (GPMC_WPN) = OFF (HIGH)
*/
compatible = "ti,am3352-gpmc";
reg = <0 0 4>; /* device IO registers */
rb-gpios = <&gpmc 0 GPIO_ACTIVE_HIGH>; /* gpmc_wait0 pin */ /* device IO registers */
ti,nand-ecc-opt = "bch8";
ti,elm-id = <&elm>;
nand-bus-width = <8>;
gpmc,device-width = <1>;
gpmc,sync-clk-ps = <0>;
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <80>;
gpmc,cs-wr-off-ns = <80>;
gpmc,adv-on-ns = <6>;
gpmc,adv-rd-off-ns = <60>;
gpmc,adv-wr-off-ns = <60>;
gpmc,we-on-ns = <10>;
gpmc,we-off-ns = <50>;
gpmc,oe-on-ns = <4>;
gpmc,oe-off-ns = <54>;
gpmc,access-ns = <40>;
gpmc,wr-access-ns = <80>;
gpmc,rd-cycle-ns = <80>;
gpmc,wr-cycle-ns = <80>;
gpmc,wait-on-read = "true";
gpmc,wait-on-write = "true";
gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <0>;
gpmc,clk-activation-ns = <0>;
gpmc,wait-monitoring-ns = <0>;
gpmc,wr-data-mux-bus-ns = <0>;
/* MTD partition table */
/* All SPL-* partitions are sized to minimal length
* which can be independently programmable. For
* NAND flash this is equal to size of erase-block */
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "NAND.SPL";
reg = <0x00000000 0x000020000>;
};
partition@1 {
label = "NAND.SPL.backup1";
reg = <0x00020000 0x00020000>;
};
partition@2 {
label = "NAND.SPL.backup2";
reg = <0x00040000 0x00020000>;
};
partition@3 {
label = "NAND.SPL.backup3";
reg = <0x00060000 0x00020000>;
};
partition@4 {
label = "NAND.u-boot-spl-os";
reg = <0x00080000 0x00040000>;
};
partition@5 {
label = "NAND.u-boot";
reg = <0x000c0000 0x00100000>;
};
partition@6 {
label = "NAND.u-boot-env";
reg = <0x001c0000 0x00020000>;
};
partition@7 {
label = "NAND.u-boot-env.backup1";
reg = <0x001e0000 0x00020000>;
};
partition@8 {
label = "NAND.kernel";
reg = <0x00200000 0x00800000>;
};
partition@9 {
label = "NAND.file-system";
reg = <0x00a00000 0x0f600000>;
};
};
};
Please let us know if we are missing anything.
Regards,
SwapniL B