Normal 0 false false false EN-US X-NONE X-NONE
Hello all,
I had a question regarding the H.264 encoding performance of the DM6467T. From the information I have seen, the part is definitely capable of encoding a single stream of either 720p60, 1080i60, 1080p30, or 1080p60. What is not clear to me is what capabilities it has for multiple streams. From the data I have seen, it should be capable of two streams of the resolutions I mentioned, except for 1080p60 obviously. In BT.656 (8b) mode, 720p60, 1080i60, and 1080p30 all would run at 148.5MHz (750x1650x60x2=148.5M, 1125x2200x30x2=148.5M, 562.5x2200x60x2=148.5M), which is under the 150MHz limit of the T part. Also, since the part is capable of doing 1080p60 encoding, I am assuming that it should be capable of moving the data and encoding two of any of the other streams (with a moderate amount software work). Does anyone know of anything that would keep this from being possible: the VPIF, DDR bandwidth, or the encoder driver/DSP? Has anyone tried this, to either success or failure? Any information would be helpful.
Thank you,
-Scott