This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The RTC support on DM368



Hi,all!

I use the DM368-MT5 IPNC as my base to develop a camera, the time and RTC is very important for my application.

but I find that the RTC is not supported very well in the DM368 IPNC. However what I do,the time will change to be the year of 2000 automatically.

I have serached the past post in this froum about RTC support on DM365, there is a post say that the RTC hadn't supported on both the software and the hardware at the end of 2009. so I want to konw is it supported very well now? How can I do to use the intenal RTC on DM368?

If the RTC on DM368 still can't be supported,what kind of external RTC chips is recommended(I mean the driver of the external RTC is integrated in the lsp and works stablely)?

btw:my DM368-MT5 IPNC software is release 2.0.0.

Thank you very much?Any help and tips will be appreciated!