Tool/software: Linux
Trying to run LTP-DDT on a custom AM3352 board. (http://processors.wiki.ti.com/index.php/LTP-DDT
I have cross-compiled it as per instructions.
I have used "make install" to get all the target-specific files copied to a output folder, that I then deploy to my target hardware.
I'm able to run the "standard" tests, e.g. "timers", "mm", "syscalls" via "./runltp -f timers"
However, if I try to run any of the TI-specific tests under "ddt", I get an error indicating that some script or binary is missing.
E.g. "runltp -f ddt/lmbench" yields the output below, which says I don't have "lmbench_tests_script.sh" installed. I get similar results with other tests (e.g. ddt/uart complains about serialcheck.sh missing)
I can find the missing scripts inside the ltp-ddt source tree.
However, these scripts are not present in the output that "make install" produces.
What am I doing wrong?
LMBENCH_L_PERF_0001 lmbench_tests_script.sh
-----------------------
LOG File: /tmp/tmp.E9JpW3
FAILED COMMAND File: /home/data/ltp-ddt/output/LTP_RUN_ON-tmp.E9JpW3.failed
TCONF COMMAND File: /home/data/ltp-ddt/output/LTP_RUN_ON-tmp.E9JpW3.tconf
Running tests.......
<<<test_start>>>
tag=LMBENCH_L_PERF_0001 stime=15[ 187.788394] LTP: starting LMBENCH_L_PERF_0001 (lmbench_tests_script.sh)
27739080
cmdline="lmbench_tests_script.sh"
contacts=""
analysis=exit
<<<test_output>>>
<<<execution_status>>>
initiation_status="pan(983): execvp of 'lmbench_tests_script.sh' (tag LMBENCH_L_PERF_0001) failed. errno:2 No such file or directory"
duration=0 termination_type=exited termination_id=2 corefile=no
cutime=0 cstime=0
<<<test_end>>>
incrementing stop
INFO: ltp-pan reported all tests PASS
LTP Version: 20180118