As per sprugr0b.pdf, ROM code supports MMC/SD cards compliant with the Multimedia Card System Specification v4.2 from the
MMCA
Technical Committee and the SD I/O Card Specification v 2 .0 from the
SD Association. Includes high-capacity (size >2GB) cards.
What is the upper bound limit (if any), for using MMC/SD card (8/16 GB) ?
Does the kernel code also support high capacity cards?
- Deepika