This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXIDK5718: Recommended power supply

Part Number: TMDXIDK5718
Other Parts Discussed in Thread: TPS659037

Hi,

1. Does TMDXIDK5718 come with power supply??

2. If not which are recommended power supply parts  for the board.  Is it expecting a regulated 5V supply?? 

One part mentioned in  EVM user guide 

""Early versions of the AM571x IDK EVM shipped with the GlobTek, Inc. external power supply with the part number TR9CA6500LCP-N, model number GT-43008-3306-1.0-T3. This external power supply is rated for

an output voltage of +5VDC with an output current up to 6.5A.""

unable to procure this. Please suggest suitable power supplies.

Also In schematics 

5V supply is fed to TPS6590377. System voltage of  TPS6590377 has a maximum rating of 5.25V and nominal voltage of 3.8V . When using an external adapter for supply how to ensure such tight specs.