hi,all. I'm using DM6446,I want to build the video_copy using CCS3.3,the video_copy is a example of xdias6.22
but I got some errors when I'm building the project. the error says "can not open file 'xdc/std.h' "
and It's the same about other header files I'm sure I've add the directory to the compiler in "option->customize->directories"
How can I fix the program?
Thanks!