Part Number: 66AK2H12
Tool/software: Code Composer Studio
We are using BIOS 6.46.05.55 and IPC 3.46.2.04 on the K2H. We have IPC configured according to an example, using the platform evmTCI6636K2H:core0 etc. However, this platform places all DSP sections in external DDR memory. Two main questions:
1) What is the most efficient way to use the C66x memory on the K2H?
- Our program is 172K with no optimization, but only 12K of computational DSP code.
- We have several large data structures which we assigned to a named section that will need to stay in DDR3, but we might like to assign smaller buffers (32K or so) to L2SRAM.
What is the best way to use the memories on the K2H?
2) How do you use specify in the cfg file how you want to allocate the DSP memories between cache, program, data or stack allocation?
Thanks,
Bruce