This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4378: QSPI driver in U-boot

Part Number: AM4378

Tool/software: Linux

Hi Biser,

Background: we only put uboot binary in our qspi flash, so our spi operation only occurs at system bootsup, and uboot burning. 

Qestion:

I am using AM4378 with uboot 201507. Our qspiflash(N25Q256) supplier MICRON suggests us porting the newest driver as my attached file.

This makes me confused, because I check uboot source code, at first, this qspiflash params is already in driver/mtd/spi/sf_params.c, secondly, the core spi call is in driver/spi/ti_qspi.c, it is a common driver, which does not distinguish the different SPI flash. Thirdly, supplier gives us a driver which looks running on MCU architecture.

In my opinion, I am no necessary to porting this provided driver to uboot, and we just follow the default driver of uboot, after all, we only operate qspiflash in uboot phrase. But I am worried about the risk.

So can you give me some professional suggestion? Any reply is precious. Thanks very much! 

Software Driver ReadMe File for:

Release history:
-Release Version 1.8 (June 2017)
 	MT25Q.c 
			Added Die erase function.

-Release Version 1.7 (June 2016)
 	MT25Q.c 
			Fixed FlashWriteEnable() variable num_of_try not initialed BUG.
		
-Release Version 1.6 (September 2015)

  MT25Q.c v1.6
  MT25Q.h v1.6
      Modify some unreasonable comments of functions.

-Release Version 1.5 (March 2014)

  MT25Q.c v1.5
      Changed FlashPemanentProtectionBitRead() to use 4bytes address
      Changed FlashPemanentProtectionBitErase() to use 4bytes address

- Release Version 1.4 (13 November 2013)

  MT25Q.h   v1.4
  MT25Q.c   v1.4
	Driver_Init() reads Discovery Parameter Table to determine
	device geometry.

	Replaced SPI_SR1_WEL (located in Serialize.h) with SPI_FLASH_WEL,
	located in MT25Q.h.
  Serialize.h
  Serialize.c

- Release Version 1.3 (04 September 2013)

  MT25Q.h   v1.3
  MT25Q.c   v1.3
	Removed "NMX_" prefix from all type definitions.

  Serialize.c
  Serialize.h
	Added to release package.

- Release Version 1.2 (27 August 2013)

  MT25Q.h   v1.2
  MT25Q.c   v1.2
        Enhanced error checking.
	Tested Suspend and Resume.
	Removed Die Erase (not supported on device).

- Release Version 1.1 (June 2013)

	Added the following functions:
	
	- FlashReadExtAddrReg()
	- FlashWriteExtAddrReg()
	- FlashEnterDeepPowerDown()
	- FlashReleaseDeepPowerDown()
	- FlashReadAdvancedSecProt()
	- FlashProgramAdvancedSecProt()
	- FlashPasswordRead()
	- FlashPasswordProgram()
	- FlashPasswordUnlock()
	- FlashPermanentProtectionBitRead()
	- FlashPermanentProtectionBitProgram()
	- FlashPermanentProtectionBitErase()
	- FlashWriteGlobalFreezeBit()
	- FlashReadGlobalFreezeBit()
	- FlashOTPProgram()
	- FlashOTPRead()
	
	Warning: this functions are provided in beta
 
  N25Q.h  v1.1
  N25Q.c  v1.1

- Release Version 1.0 (February 2013)

  Full alpha version
 
  N25Q.h  v1.0
  N25Q.c  v1.0
 
- Release Version 0.1 (January 2013)

  Alpha version with a subset of commands implemented
 
  N25Q.h  v0.1
  N25Q.c  v0.1
 
 
Note: Added support for N25Q256A8. The driver supports both standard N25Q and new N25Q256A8X command set.

MT25Q.c

  • The qspi_flash interface is standard and the u-boot drivers are written based on this assumption.  Majority of flash devices can be supported without implementing devices specific modifications.  Therefore, you shouldn't have to port any code.