This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: CMB interface issue

Part Number: AM5728
Other Parts Discussed in Thread: PCM1864

Hi ,

In my present project I am working on interfacing Circular Microphone Board(CMB) with GPEVM AM572x sitara processor.

I am using McASP7 lines as audio in lines, I tested the interface on 2 microphones and is working as expected.

The audio data is passing through BF, AEC , MSS algorithms and I am able to listen  clean audio out through audio out jack on EVM.

I am able to access 2 McASP7 Data in port pins on EVM, hence I want to interface 4 microphones from CMB.

I am configuring to work with 2 serializers, pin mux for both pins are proper. Rx, Tx, signal processing buffer lengths seems to be proper.

But when I test the interface of 4 microphones with AM572x through 2 McASP7 serializers, I am unable to listen to clean audio, it is  not completely mute,

I am able to listen the distorted audio, there is no background noise but audio is distorted, what would be possible issue?

I am using K2G interface with CMB as reference code.

Thanks in advance,

-Janardan M