Part Number: AM3358
Tool/software: Linux
Hello,
I am using am335x custom board base on beanglebone design (linux kernel 4.9.69).
I have two custom board, when executing ifconfig command one is working file,
and another board, get problem eth0 IP address is missing. pls help.
root@am335x-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr C4:F3:12:80:EA:36
inet6 addr: fe80::c6f3:12ff:fe80:ea36%763860/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:30 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:5571 (5.4 KiB)
Interrupt:175
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1%763860/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:3 errors:0 dropped:0 overruns:0 frame:0
TX packets:3 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:312 (312.0 B) TX bytes:312 (312.0 B)
usb0 Link encap:Ethernet HWaddr 2A:27:2D:65:34:67
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
wlan0 Link encap:Ethernet HWaddr 50:33:8B:D8:0D:1F
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Here if the log when I run ifup eth0
root@am335x-evm:~# ifup eth0
udhcpc (v1.24.1) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background