This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Driving a CCIR601/656 LCD from Am1806 LCD controller

Other Parts Discussed in Thread: AM1806

It is not clear to me if the LCD controller can output a CCIR601 or CCIR656 8-bit format.  We're using a 320x240 color LCD panel which has either 24-bit RGB interface or a CCIR601/656 8-bit interface (Am1806 only has a 16-bit output for the LCD interface).  Am I correct in assuming that the microprocessor's LCD would be used in a "LCD Raster-Mode Passive" setting (Figure 6-54, page 188 of data sheet) to output a CCIR601 or CCIR656 format ?